This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25170EVM: can't fully charge a Li-Ion cell

Part Number: BQ25170EVM

Tool/software:

Hey

i bought the bq25170evm board to use in a bms system, i have hade some problems with it not charging the batteris i am using fully "CL-18650-MH1/1S2P".

i have tried with a single cell and it just stops charging when it reaches around 3.6 V, i have set it to 4.2 "#5 / R5 / 27k ohm 4.2V / 1-Cell Li-Ion".

i am a bit lost right now i have been trying to figure it out for a few days now and i don't know what to do at this point.

is there someone that could point me to what i am possibly doing wrong ??

thanks in advance

  • Hi Jacob

    Couple of things to check:

    1.) Double check the resistance of VSET (TP7) to GND, verify 27k ohms

    2.) Do you any current meters at input or output?  They have caused problems with other customers.

    3.) Double check the Jumper setting, see table 2-1 from User Guide.

  • Hey Bill

    i just double checked all the things you where asking about.

    1. yes there is 27K on VSET (TP7)

    2. No i only have a volt meter on the output to see the battery voltage.

    3. all jumpers are setup as shown in table 2-1

    but it still does stop charging when it hits 3V6.

    the only diffence between what is said in 2.3 test instructions and my setup is that i don't have a battery simulator. i do use a normal 18650 samsung cell.

    could that be the problem ??

  • Hi Jacob

    Can you send photo of the board and test set up?

    What it the STAT LED behavior, is it ON during charge then turns OFF?

    Also ISET pin voltage will indicate current to battery, what is ISET voltage?

  • Hey bill

    i do belive i have found the problem, i do belive that i hade a bad NTC when i removed that and just used a 10K resistor it has worked fine for the last 8-9 hours.

    but i can still send the other information if you would like

  • No -- go ahead and test with the 10k for now.