Tool/software:
We are designing a USB3 Hub with PD that includes the TPS65982DMC combined with the TPS65988DH similar to the system diagram from the datasheet of the DMC:
The TPS65988DH can be configured with the Application Customization Tool. I have version 6.1.4.
How can I configure the TPS65982DMC? This is not included in the tool above.
On our board both - the TPS65988DH and the TPS65982DMC - have a SPI flash to save their config. Can the flash of the TPS65988DH be updated TPS65982DMC via I2C?
If yes - is there a tool to test and configure this setup?
Thanks.