Other Parts Discussed in Thread: BQ25750
Tool/software:
Hi all,
It is not clear from the BQ25756 datasheet what will be the output voltage of the charger in case that the input voltage is different then the battery voltage (higher or lower).
Is that depends to the battery regulation circuit configuration (FB, FBG)?.
One may conclude from Figure 9-1 that in 12V battery case the battery regulation configuration forces output voltage to be the maximum battery voltage - 16.8V.. What does it means? If this will be the charger output voltage independent to the battery voltage, there could be situation that the battery voltage will be only 8V and when disconnecting the external power the charger output voltage will abruptly jump from 16.8V to 8V - bad for the load.
Thanks.