Tool/software:
Hi team,
Could you please help review the LP8865Y-Q1 schematic and give some comments?
Customers are currently switching the R56 resistance to 11K and the LED can be illuminated when the input is 12-18V, but when the input voltage is greater than 20V, The LED cannot be illuminated.
9~32V input; 1A output current, 13V LED output.
Regards,
Ivy