This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM63610: Regarding enabling the TPSM63610 through FPGA

Part Number: TPSM63610


Tool/software:

Hello all,

I am using TPSM63610 in my project for three applications (28V to 12V, 28V to 8.5V and 12V to 4V conversion). In the datasheet (reference schematic in the datasheet) as well in TI WEBENCH circuit designer, the IC is being enabled through Vin only. I want to enable it through the FPGA. My FPGA I/O banks are operating at 3.3V.

Can I directly connect a signal from FPGA I/O bank to the enable pin of the IC TPSM63610? If not, please suggest how to connect for all three applications (28V to 12V, 28V to 8.5V and 12V to 4V conversion).

Regards, 

Sahil