Other Parts Discussed in Thread: TPS65994QFNEVM
Tool/software:
Dear Team,
my customer wishes support in creating the FW for the TPS65994AD. His wish is to use the USB-C Charging capabilities of port 1 of two, not port 2. He needs 20V and 4A to charge the laptop. It should be charged from an external source via USB-C but should also put out 5V / 3A to external devices.
I also looped my customers R&D on this thread: @Alex: Can you please comment on which parameters of the configuration GUI you need help with?
Thanks, RWE