Tool/software:
We have custom hardware with bq35100 installed. Current hardware unfortunately does NOT support open open circuit voltage calibration.
1)Can I calibrate voltage with current flowing? What are the effects? I may be able to put the device in a low power state to get the current consumption way down but it won't be 0.
2)Any issue with using a power supply in place of the battery for this calibration procedure?
3)For the current calibration I was just going to put the device in a while loop to maintain steady current consumption and calibrate using a power supply-Again any issues here?
4)Whats the point of the board/cc_offset calibration, why would I want to 0 out the current if in fact current is flowing? Wouldn't I have to reaccount for that in my power/discharge calculations...