Other Parts Discussed in Thread: UCC28C41, UCC28C44, UCC28C45
Tool/software:
Hi,
We are using the LM5021-2 for a two transistor forward. Do you think this is OK? At startup and overload, the thing will obviously go into 50% duty cycle, and if there is tolerance such that max duty cycle is actually 51%, then it will staircase saturate. So can you garantee that LM5021-2 is definetely no more than 50.0% duty cycle?