Other Parts Discussed in Thread: BQ25150, SN74LVC1G126
Tool/software:
I want to use a push button connected to TS/MR to exit ship mode but also be able to read the push button state on the MCU.
Looking at the datasheet it seems tWAKE1 can only be set to 300ms and I really need to be able to detect faster events so I can't rely on the BQ25180 to do it.
What circuit can I use to connect a push button to TS/MR so end users can exit ship mode and also reliably read out the button with an MCU where it's used as a navigation button?
In the linked thread a circuit is given with two FETs and a push button that connects to VDD, however when in ship mode it seems to me VDD isn't available and that circuit uses VDD to drive the gate but VDD won't be available since we're in ship mode?
Ideally I'd want the button to read high on the MCU side when pressed.
If it helps: TS function won't be needed so that will be tied to a 10k resistor as suggested in the datasheet.