Tool/software:
Hi Team,
Currently, I'm using the TPS63805 buck-boost to stabilize the input 3.3V to output 3.3V,
and the output is facing unstable issue during the power-on (as below pic),
the output appears that it stay at 1.2V for about 200us before continuing to ramp up,
I tried to measure the L(input/output), and it doesn’t work during this period, the Tramp and Tdelay is 4.47ms and 327.8us


After I separated the EN and VIN pin, we can see the issue will be solved,
but just want to confirm, the reference in the SPEC mentioned the Vin can connect with the EN pin,
In our measurement today, we know that delaying or reducing the enabled voltage will solve this issue,
But can I understand what might be causing this issue, even though we have followed the reference circuit? Thank you.
EN pin input after the Vin

Reduce the EN pin to 1.8V