Tool/software:
Dear TI experts,
My customer found the issue about adapter detection using BQ24297. Please see the detailed description below.
1. First I attach the schematic for your convenience.
2. They use 4 lines USB A-to-C cable. (Device side is type C, and adapter(or laptop USB) side is type A.)
3. When R82 and R83 is attached (D+ and D- is connected)
3-1. tested PD adapter, Samsung adapter, Normal 5V/1A adapter, 2 different power banks are connected to VBUS => charged as 950mA current.
3-2. tested Apple adapter, DC Power supply(using only VCC and GND, not using D+ and D-) => charged as 450mA current, but sometimes charged as 950mA current. (I don't know why yet.)
3-3. tested connecting VBUS to laptop USB (Samsung, LG) using 4 lines A-to-C cable => not charged, still 5V is present. STAT pin is high. (charging is complete even not completed battery charging)
3-4. tested connecting VBUS to laptop USB (Samsung, LG) using 2 lines A-to-C cable (only 5V and GND) => charged as 950mA current.
4. When R82 and R83 is not attached (D+ and D- is not connected)
4-1. tested PD adapter, Samsung adapter, Normal 5V/1A adapter, 2 different power banks are connected to VBUS (both using 2 lines A-to-C cable and 4 lines A-to-C cable) => charged as 450mA current. but sometimes charged as 950mA current. (I don't know why yet.)
4-2. tested connecting VBUS to laptop USB (Samsung, LG) (both using 2 lines A-to-C cable and 4 lines A-to-C cable) => charged as 450mA current.
(** 2 lines A-to-C cable is which D+/D- shorted on device side.)
Anyway My customer have a question especially about the result of 3-3 and 3-4.
Could you check the possibility of each scenarios are right or not?
And please let me know if you need more information about it.
Best regards,
Chase