Tool/software:
Hi,
I'm looking at the datasheet of the BQ25756 and it states that it can go up to 14 cells for a li-ion battery (16 for LiFePO4). At the same time, it is specified to work for a battery voltage of up to 70V. But considering a maximum Li-ion cell voltage of 4.2V per cell, a 16 cell battery pack would only reach 67.2V. Does this mean that the BQ25656 can also be used for a 16 cell Li-ion battery pack?