Part Number: TPS923655
Other Parts Discussed in Thread: TPS923652, TPS923653,
Tool/software:
We'd like to use this chip to power an 18v/500mA COB, using the chip in a boost configuration.
In using the Excel-based tool, when using 5V as input, the efficiency is only 85% and temperature rise is ~30 degrees.
With 9v input, the efficiency leaps to 91% and temperature rise is only ~9 degrees.
Does it make sense with 5v input to pursue an additional external boost stage to 9v or 12v? Otherwise it seems like the device is going to run quite hot.
Many thanks!