This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5066: LM5066I

Part Number: LM5066


Tool/software:

Dears,

LM5066 Pin monitoring accuracy is +/- 4.5%, and LM5066I is +/-2.5%.

According to our experiment result, the accuracy of light load is more than the specification +/-4.5 or +/-2.5, and the Pin accuracy might be more than 10% if delta Vsense is less 3mV.

the delta Vsense is equal to Vsens+ - Vsense-.

Could you provide with the curve of the accuracy vs delta Vsense?

which factor is the major part to let accuracy worse?


Thanks.