Other Parts Discussed in Thread: UCC5390
Tool/software:
Hi team,
Our EVM only showed wrong pin out of UCC5390 on the output. Can you help provide reference schematic and layout when driving two parallel SIC FET by using UCC5390E?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
Our EVM only showed wrong pin out of UCC5390 on the output. Can you help provide reference schematic and layout when driving two parallel SIC FET by using UCC5390E?
Hi Zoe,
The EVM is configurable to work for either package variant.
To drive two parallel FETs with the E version, they could try something like this:
Best regards,
Sean
Hi sean,
Do we have recommendation layout on Clamp pin for driving two SIC in parallel?
Hi Zoe,
If you use the UCC5350M, you should put 1-2.2Ω between CLAMP and each gate. That will still be below the inductance floor of the gate loop impedance at high frequency, but it will help soften any FET mismatch during turn-on due to Vth process differences.
Best regards,
Sean
Clamp Circuit suggestion:
Miller pull down impedance: Injection is usually >50MHz