Part Number: LM5156
Other Parts Discussed in Thread: LMR36503
Tool/software:
I would like to design a boost circuit using LM5156.
VIN=10 - 42V
IOUT = 1A
VOUT = 48V, 36V, 24V
The thinking here is that I can use some FETs to modify the feedback resistors to select output voltage during runtime. Obviously if the circuit was at the highest input voltage range the lower output voltage setpoints would not be regulating and would just be in passthrough mode of the controller.
What are the implications of compensation?
What would the correct design approach be? For example, design per datasheet procedure at minimum VIN (10V) and maximum VOUT (48V), and should the other combinations just work?
I would appreciate any feedback on this topic.
Thanks!