Other Parts Discussed in Thread: LM7480,
Tool/software:
Can a LM7480-Q1 be used on a 3.3V output circuit, as the VS > 3V for operation? As the 3.3V output would fall in a current limit situation, would supplying the VS pin form an external housekeeping source be valid, or does this cause issues with the charge pump circuitry. With an eternal VS supply, the VS > Vin (pin A)? It looks like this can be done, as page of the datasheet, shows a zener generated supply in the figure at the lower right "Ideal Diode with 200-V Load Dump Protection". In this particular instance VS < Vin. I am not interested in the LM7480 going into UVLO. I would prefer to have the 3.3V supply fold-back and the diode controller follow along, behaving like a real diode.