This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561EVM-011: bqstudio Chem_ID 2162, NiCoMn/carbon ?

Part Number: BQ27Z561EVM-011


Tool/software:

Full disclosure I'm not a battery expert, but is that chemica makeup correct for the INR18650-35 (3400mAh)? No Li mentioned which is why I ask. It is a lithium battery according to the data sheet.

  • Hello Craig,

    Yes, the chemical description is correct. Li-ion is a very generic term for a battery chemistry. NiCoMn is a type of Li-ion chemistry (it's technically Li-NiCoMn O2, NiCoMn is just the short hand notation). Other types of Li-ion battery chemistries are NMC, LFP, and LTO.

    Regards,

    Nick Richards