Part Number: LM5156H
Tool/software:
Hello guys,
I am designing a boost flyback controller using LM5156HPWPR. So far everything work fine except for the UVLO low voltage threshold is not following my calculations:
My settings are as below:
Vsupply(on) = 7.8V
Vsupply(off) = 7.0V
By calculations, here are the values I got:
RUVLOT = 100k
RUVLOB = 23.2k
From my test, I can get the driver to turn on correctly at +V_BATT = 7.8V. However, the driver will immediately stop driving when the voltage drops to +V_BATT = 7.7V and below.
What is the issue here?
I have done the following:
- Reconfirm the values for soldered RUVLOT & RUVLOB.
- Swap RUVLOB GND to PGND and AGND.
- Resolder LM5156H IC.
- Replaced LM5156H IC.
Here's my schematic for reference: