This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713: BQ25713: need a wait time between two commands

Part Number: BQ25713

Tool/software:

Hi,

In the application I am developping I noticed that if I send two commands too close to each other, the first one is not executed.

e.g : I request a set charge then a ADC conversion, the set charge is not done. But if I wait a certain amount of time (100ms works) between the two, the set charge is done.

Is it possible ? If yes is it possible to have worst case wait ?

Regards