Part Number: TPS7A39
Tool/software:
Ti Team,
Planning to use TPS7A39 dual regulator.We need +5V at OUTP (pin10) and -5V at OUTN (Pin 6). Below is the questions:
1.Do I need to give +12V @INP (Pin 1) and -12V @INN(Pin 5) ?
2.If I give +12V @INP (Pin 1) and -10V @INN(Pin 5) ,then is it possible to get +5V at OUTP (pin10) and -5V at OUTN (Pin 6) ?
3.With any input voltage range ,Is output current is 150mA available at both the channels?
Thanks and Regards
Prashanth Pai B