Tool/software:
Hi folks.
Would I be able to get a quick review on this schematic for the BQ25895?
My requirements:
- Input is via USB-C, so VBUS would be powered at 5 V from 500 mA and above.
- Power draw on VCC will never exceed 600 mA.
- USB OTG must be disabled and will not be used in the future.
- Battery charging must be enabled, unless disabled by the microcontroller by pulling PWR_CE high.
- I calculate that the 330 Ω resistor between ILIM and GND will limit charging current to the battery to between 0.96 - 1.18 A (around 1.07 A typical). To confirm, am I correct?
Many thanks!