Other Parts Discussed in Thread: LM5117, LM5060, TPS2493, CSD, CSD19536KTT
Tool/software:
Hello,
I need to add a high switch switch in the output of a variable power supply implemented using LM5117.
To drive the series N-mosfet, we can use a eFuse driver or High side driver like LM5060 or 66, TPS2493, TPS4811 etc.
No protections are required but can be used if available in the driver we finalize. Reverse flow is not required. (4811 in attached schematic, but any can be used)
The output of the switcher is required from 0.5 - 50Vdc, input is 55V from an earlier stage.
Since the driver cannot operate at that voltage, is it okay to power it from the Vin of the switcher which is 55V?
1. LM5060 or TPS4811 Vin would be 55V but mosfet drain will be at 0.5 to 50V. Will this work or cause any problems?
2. Series current will be max 20A @ 50V. Since mosfet is not switched rapidly, can we use an SMD mosfet from the CSD195xx family,
e.g. 80V, 100A in TO-263 or is a TO-220 device recommended from dissipation requirements.
3. What is the recommended rating for Qd?
Thanks and regards,
Tanmay Sutaria.