Other Parts Discussed in Thread: UCC28951
Tool/software:
Hello Team,
Spec: Vin - 80 to 120V , Vout - 13.8V , Irated - 35A , Transformer TR - 4.5:1:1 , Fsw - 150kHz, 0.36V @ DCM ,
Following observation taken with 50% of scaled operational range.
- We are observing Vout oscillation , when are operating with light load current of 2A to 4A (actual rating 35A).
- We could observe COMP pin voltage droping below 0.8V & coming back after few cycle, so it shows burst mode operation.
- As we are approaching maximum input voltage & same light load condition, Observing too much oscillation at Vout, COMP , SS & CS. Still Vout regulation happens as expected.
- If load current exceeds 15% to 20% not observing this noise oscillation issue.
- How can we overcome this noise issue in the light load operation?
Thanks for your support in advance.
Rgds,
Babu