Other Parts Discussed in Thread: BQ79616
Tool/software:
Hi Team,
Customer is designing BQ79616 with BQ79600. Please review the schematic below and let me know if there are any points to change or not.
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
Customer is designing BQ79616 with BQ79600. Please review the schematic below and let me know if there are any points to change or not.
Regards,
Hi Jeffrey,
I will get with the team to review the schematic. I will provide an update in the coming days.
Best regards,
Barry
Hi Jeffrey,
LDO Power Tree:
DVDD needs 2.2uF not 1uF
AVDD, CVDD, REFHP, NEG5V, TSREF, BAT, and LDOIN have datasheet capacitor values which is fine.
LDOIN-NPNB LDO circuit
Has good NPNs, and good RNPN/CNPN
GPIOs:
Unused GPIOs should be grounded with a 10kohm resistor instead of being shorted to GND.
GPIO 1 and 2 are fine
Daisy Chain:
The daisy has the recommend BOM with transformers so that is fine.
VCCB Connections:
The BOM looks fine.
Best regards,
Barry Zhang
Hi Barry,
Thanks for your design review. Additionally, customer wants to know if inductors of L1/L2 can be used on daisy chain line. There is not used the transformer on EVM schematic part4 below. Please let me know the correct application about this.
Regards,
Hi Jeffrey,
A choke can be used instead of a transformer for the daisy chain isolation. Generally speaking, however, we recommend a transformer for better robustness.
Best regards,
Barry