This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS50601-SP: Questions about datasheet

Part Number: TPS50601-SP

Tool/software:

Hello,

My customer has questions about the datasheet as follows.

Q1:
At the equation (20) on page 29, L1 is Lo in the Figure 29 on page 28?

Q2:
Referring to Table 2, at the equation (20) on page 29, calculated L1 is about 5.46uH, not 2.78uH when KIND = 0.1. How can you get the 2.78uH here?

Q3:
In 9.2.2.8 of the datasheet, what are the R5 and R6? Are they R1 and R2 in the Figure 29?

Q4:
At the equation (37), what is the R2? Which figure of the datasheet should be referred about the R2 here?

Q5:
At the equation (368), what is the C3? Which figure of the datasheet should be referred about the C3 here?

Best regards,

K.Hirano