Part Number: UCC28750
Tool/software:
Hello, I have designed a power supply using UCC287506 to be operated on 100kHz, 12 watt output power. I am facing an issue during startup at full load. My observation is that during startup the controller is switching at 50kHz, which is causing it to trigger over power protection.
I tried to reduce the Rcs (2.2E || 2.2E) by half during turn on and changed it back to the original vale (Rcs = 2.2E) then the circuit is working. But when im keeping RCS = 2.2E the circuit is going in hiccup mode.