This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25622: What's the absolute maximum current for the HS/LSFET ?

Part Number: BQ25622

Tool/software:

Hi, 

I'm doing some calculations for the BQ25622 charger IC. What I'm trying to figure out is the allowable maximum ripple current of the design. The datasheet recommends 20-40% ripple vs average, but what's the limit ? How much can the HS and LS fets take ? I have a rather large stock of components that would give about 85% ripple current @2.5A output current. 

The datasheets mentions a maximum recommended Isw current of 3.5A. Is that RMS or peak current ?


Appreciate any answers.