I am working on a design of a Linear LED light that uses 2 strings of 80 30ma 3.2V LEDs per module, and up to 5 modules in series. This will run off universal line input (85 – 265 Vac) The design must be UL Class 2 compatible so I caint have a HV string of LEDs. The 2 LED strings must be individually dimmable via a PWM signal. The preliminary plan was to use the UCC28810 for PFC flyback and then 2 buck converters to control the LED current. The other option would be to use a C2000 to do all of the control. I would like not to have to use a C2000 if possible, but if it is not realistically possible with all analog components I will make the switch. Another constraint is that the overall system efficiency must be higher than 85%. Does anyone know of a solution to this?