This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25751EVM: App Customization Tool/GUI unable to connect to EVM

Part Number: TPS25751EVM
Other Parts Discussed in Thread: TPS25751

Tool/software:

Hello,

I am trying to use the USBCPD Application Customization Tool GUI to configure the TPS25751 chip on the EVM, but I'm getting an error. The status ribbon at the bottom of the window shows "Error: failed to connect: No port found. Please plug your target device into your computer's USB port, and click the connect icon on the left."

My device is plugged in to my PC via a USB-A/C cable which supports data. The GUI was able to detect another device that I had connected to this port, but not the EVM.
I have tried using both the web tool and the natively installed one but got the same result. Only one instance of the tool is running.

Is there something else I can do to resolve or troubleshoot this issue?