Tool/software:
We plan to use the BQ27621 to measure battery voltage.
However, in some use cases, the battery connector may be connected to a 5V DC power source instead of a battery.
In this case, a voltage of about 5.0 to 5.25 V is applied to the VBAT pin.
Abolute Maximum Ratings for VBAT are up to 6V.
However, the VBAT of the LDO Regulator and ADC is limited to 4.5V.
Will connecting 5V to VBAT cause IC destruction?