Part Number: TMDSEVM6657
Other Parts Discussed in Thread: UCD9222, UCD7242
Tool/software:

I have a few questions regarding UCD9222.
In the circuit diagram, the signal that controls UCD9222 is as follows.
1. Connect FPGA to PMBUS interface
2. Connect to DSP and VID interface
3. Connect via JTAG interface
There are three cases as above.
In this case, I have the following questions.
The hardware configuration is DSP + UCD9222+UCD7242 structure.
1. Is there any problem in operating UCD9222 with DSP's VID interface without PMBUS and JTAG interface?
2. If not, how to control and operate UCD9222 through PMBUS.
3. If not, install and operate the firmware of UCD9222 through JTAG.
Please ask for help. thank you