hi,
I am working on a battery charger based on the BQ24600 with 4-cell Li-phosphate,and each battery is 3.2V/50Ah. Later i kow the BQ24620, but there is external circuit with MCU and ADC components to monitor and protect the battery,so it doesn't matter to use the bq24600 or the bq24620.
Input voltage: 24VDC
In the time earlier i tested the bq24600 in a PCB board with bad layout, but it works well except the heat conduction.So i used the same circuit and the same components in the new board,but it can not work.
The output voltage is just only 0.8V, and the state led blink.
So i get the waveform on the high side driver and the low side driver. i found they were always been turned off.
The VREF pin is 3.269V, CE connect to the VREF, S pin is 1.6V, ISET pin is 1V. REGN pin is 6V, and the bootstrap capacitor is 4.62V,
Because the output voltage is almost 0,the VFB pin is almost 0.
Then I disconnect the HIDRV pin to the gate of high side MOSFET, both high side driver and low side driver output nothing.
I replaced the bq24600 and the mosfet(SIR426) , nothing changed. I need some suggestions
Thank you.
Lee