Tool/software:
Hi,
in the DS section 8.2.2.1 the calculation of Cout2 and Cout3 are the capacitor between (COM−VEE) and (VDD−COM) respectively.
If the module is used at single output configuration such as (VDD – VEE) 18 V to 25 V, then how much is the maximum capacitive load the module can handle during power up with the maximum resistive load ?
BR,
Stefan