Other Parts Discussed in Thread: AM6411, , TPS746
Tool/software:
Hi,
AM6411 is using TLV75518P and TPS74601. The design requirement is to check the slew rate less than 18mV/us.
And we could only see 3.3V power up waveform in the datasheet.
Thus, we want to check with BU for the 1.8V output slew rate of both of TLV75518P and TPS74601, please advise.
Additional question is, may I increase output capacitance to reduce startup slew rate?
Thanks and Best regards,
Tiger
P.S:
- TLV755P startup slew rate= 11mV/uS
- TPS74601 startup slew rate= 11mV/uS (or 11.8mV/uS if the raising time is 280uS)