This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25751: Can't sink 3A current

Part Number: TPS25751

Tool/software:

Hi Team,

As title, we are designing a power bank, but the typeC port sink current is only 1A when we connect to typeC adapter.(5V) We checked the 0x29[1:0] and the data is 2h which means it should be 3A.

Not sure which register that we need to check or write. May you help give us some suggestions? Thank you.

Ps. The current is providing to our battery charger. We also use the 12V power supply Vin and the charge current can be up to 3A. So charger may not be a factor limit the sink current.

Regards,

Roy

  • Hi Roy,

    Can you provide a PD log in this case?

    The PD does not control the nor limit current, so if you are only seeing 1A being pulled, the limitation would be somewhere else.

    Thank you,

    Kevin

  • Hi Kevin,

    Sorry. My question is that we would like charge my device by using TPS25751 typeC port. The typeC source current is only 700mA. Currently, I'm checking with the 5V power device, but may you help check my typeC setting(source)?

    [2024-06-27 09:52:50.462] [JET/DEBUG]uart_thread.c:doCommand()(741):ra device:0
    [2024-06-27 09:52:50.464] [JET/DEBUG]i2c.c:readAllReg()(564):i2cType:0 i2c_addr:0x20
    [2024-06-27 09:52:50.479] [JET/DEBUG]i2c.c:readAllReg()(575):[20][3] Buf[0]:0x4  //4byte
    [2024-06-27 09:52:50.479] [JET/DEBUG]i2c.c:readAllReg()(575):[20][3] Buf[1]:0x41 //A
    [2024-06-27 09:52:50.495] [JET/DEBUG]i2c.c:readAllReg()(575):[20][3] Buf[2]:0x50 //P
    [2024-06-27 09:52:50.495] [JET/DEBUG]i2c.c:readAllReg()(575):[20][3] Buf[3]:0x50 //P
    [2024-06-27 09:52:50.500] [JET/DEBUG]i2c.c:readAllReg()(575):[20][3] Buf[4]:0x20 // LSB
    [2024-06-27 09:52:50.520] [JET/DEBUG]i2c.c:readAllReg()(575):[20][4] Buf[0]:0x4
    [2024-06-27 09:52:50.527] [JET/DEBUG]i2c.c:readAllReg()(575):[20][4] Buf[1]:0x49
    [2024-06-27 09:52:50.531] [JET/DEBUG]i2c.c:readAllReg()(575):[20][4] Buf[2]:0x32
    [2024-06-27 09:52:50.549] [JET/DEBUG]i2c.c:readAllReg()(575):[20][4] Buf[3]:0x43
    [2024-06-27 09:52:50.549] [JET/DEBUG]i2c.c:readAllReg()(575):[20][4] Buf[4]:0x20
    [2024-06-27 09:52:51.567] [JET/DEBUG]i2c.c:readAllReg()(575):[20][6] Buf[0]:0x8
    [2024-06-27 09:52:51.572] [JET/DEBUG]i2c.c:readAllReg()(575):[20][6] Buf[1]:0x0
    [2024-06-27 09:52:51.583] [JET/DEBUG]i2c.c:readAllReg()(575):[20][6] Buf[2]:0x0
    [2024-06-27 09:52:51.593] [JET/DEBUG]i2c.c:readAllReg()(575):[20][6] Buf[3]:0x0
    [2024-06-27 09:52:51.596] [JET/DEBUG]i2c.c:readAllReg()(575):[20][6] Buf[4]:0x0
    [2024-06-27 09:52:51.611] [JET/DEBUG]i2c.c:readAllReg()(575):[20][6] Buf[5]:0x0
    [2024-06-27 09:52:51.611] [JET/DEBUG]i2c.c:readAllReg()(575):[20][6] Buf[6]:0x0
    [2024-06-27 09:52:51.614] [JET/DEBUG]i2c.c:readAllReg()(575):[20][6] Buf[7]:0x0
    [2024-06-27 09:52:51.630] [JET/DEBUG]i2c.c:readAllReg()(575):[20][6] Buf[8]:0x0
    [2024-06-27 09:52:51.635] [JET/DEBUG]i2c.c:readAllReg()(575):[20][8] Buf[0]:0x4
    [2024-06-27 09:52:51.646] [JET/DEBUG]i2c.c:readAllReg()(575):[20][8] Buf[1]:0x0
    [2024-06-27 09:52:51.654] [JET/DEBUG]i2c.c:readAllReg()(575):[20][8] Buf[2]:0x0
    [2024-06-27 09:52:51.664] [JET/DEBUG]i2c.c:readAllReg()(575):[20][8] Buf[3]:0x0
    [2024-06-27 09:52:51.666] [JET/DEBUG]i2c.c:readAllReg()(575):[20][8] Buf[4]:0x0
    [2024-06-27 09:52:57.727] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[0]:0x40
    [2024-06-27 09:52:57.733] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[1]:0x0
    [2024-06-27 09:52:57.743] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[2]:0x0
    [2024-06-27 09:52:57.754] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[3]:0x0
    [2024-06-27 09:52:57.754] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[4]:0x0
    [2024-06-27 09:52:57.765] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[5]:0x1
    [2024-06-27 09:52:57.769] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[6]:0x2
    [2024-06-27 09:52:57.784] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[7]:0x5
    [2024-06-27 09:52:57.784] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[8]:0xB1
    [2024-06-27 09:52:57.787] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[9]:0xA8
    [2024-06-27 09:52:57.803] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[10]:0x2E
    [2024-06-27 09:52:57.803] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[11]:0x6D
    [2024-06-27 09:52:57.811] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[12]:0xB4
    [2024-06-27 09:52:57.820] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[13]:0x43
    [2024-06-27 09:52:57.822] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[14]:0xED
    [2024-06-27 09:52:57.837] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[15]:0xB9
    [2024-06-27 09:52:57.837] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[16]:0xAD
    [2024-06-27 09:52:57.840] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[17]:0x6
    [2024-06-27 09:52:57.855] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[18]:0x80
    [2024-06-27 09:52:57.855] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[19]:0x27
    [2024-06-27 09:52:57.868] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[20]:0x0
    [2024-06-27 09:52:57.871] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[21]:0x11
    [2024-06-27 09:52:57.884] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[22]:0x9
    [2024-06-27 09:52:57.887] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[23]:0xF8
    [2024-06-27 09:52:57.887] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[24]:0x3
    [2024-06-27 09:52:57.902] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[25]:0x0
    [2024-06-27 09:52:57.902] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[26]:0x1
    [2024-06-27 09:52:57.910] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[27]:0x19
    [2024-06-27 09:52:57.922] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[28]:0x3
    [2024-06-27 09:52:57.922] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[29]:0x0
    [2024-06-27 09:52:57.937] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[30]:0x0
    [2024-06-27 09:52:57.937] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[31]:0x96
    [2024-06-27 09:52:57.951] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[32]:0x52
    [2024-06-27 09:52:57.954] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[33]:0x37
    [2024-06-27 09:52:57.954] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[34]:0x96
    [2024-06-27 09:52:57.965] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[35]:0xE6
    [2024-06-27 09:52:57.968] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[36]:0x52
    [2024-06-27 09:52:57.986] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[37]:0x37
    [2024-06-27 09:52:57.986] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[38]:0x0
    [2024-06-27 09:52:57.986] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[39]:0x0
    [2024-06-27 09:52:57.996] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[40]:0x0
    [2024-06-27 09:52:58.006] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[41]:0x0
    [2024-06-27 09:52:58.008] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[42]:0x0
    [2024-06-27 09:52:58.023] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[43]:0x0
    [2024-06-27 09:52:58.023] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[44]:0x0
    [2024-06-27 09:52:58.026] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[45]:0x0
    [2024-06-27 09:52:58.041] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[46]:0x0
    [2024-06-27 09:52:58.041] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[47]:0x0
    [2024-06-27 09:52:58.051] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[48]:0x0
    [2024-06-27 09:52:58.053] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[49]:0x0
    [2024-06-27 09:52:58.070] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[50]:0x0
    [2024-06-27 09:52:58.070] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[51]:0x0
    [2024-06-27 09:52:58.072] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[52]:0x0
    [2024-06-27 09:52:58.087] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[53]:0x0
    [2024-06-27 09:52:58.087] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[54]:0x0
    [2024-06-27 09:52:58.097] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[55]:0x0
    [2024-06-27 09:52:58.100] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[56]:0x0
    [2024-06-27 09:52:58.108] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[57]:0x0
    [2024-06-27 09:52:58.118] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[58]:0x0
    [2024-06-27 09:52:58.120] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[59]:0x0
    [2024-06-27 09:52:58.134] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[60]:0x0
    [2024-06-27 09:52:58.134] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[61]:0x0
    [2024-06-27 09:52:58.142] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[62]:0x0
    [2024-06-27 09:52:58.145] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[63]:0x0
    [2024-06-27 09:52:58.161] [JET/DEBUG]i2c.c:readAllReg()(575):[20][9] Buf[64]:0x0
    [2024-06-27 09:52:58.169] [JET/DEBUG]i2c.c:readAllReg()(575):[20][D] Buf[0]:0x4
    [2024-06-27 09:52:58.175] [JET/DEBUG]i2c.c:readAllReg()(575):[20][D] Buf[1]:0xF8
    [2024-06-27 09:52:58.185] [JET/DEBUG]i2c.c:readAllReg()(575):[20][D] Buf[2]:0x19
    [2024-06-27 09:52:58.193] [JET/DEBUG]i2c.c:readAllReg()(575):[20][D] Buf[3]:0x0
    [2024-06-27 09:52:58.195] [JET/DEBUG]i2c.c:readAllReg()(575):[20][D] Buf[4]:0x0
    [2024-06-27 09:52:58.211] [JET/DEBUG]i2c.c:readAllReg()(575):[20][F] Buf[0]:0x4
    [2024-06-27 09:52:58.223] [JET/DEBUG]i2c.c:readAllReg()(575):[20][F] Buf[1]:0x53
    [2024-06-27 09:52:58.225] [JET/DEBUG]i2c.c:readAllReg()(575):[20][F] Buf[2]:0x11
    [2024-06-27 09:52:58.241] [JET/DEBUG]i2c.c:readAllReg()(575):[20][F] Buf[3]:0x9
    [2024-06-27 09:52:58.241] [JET/DEBUG]i2c.c:readAllReg()(575):[20][F] Buf[4]:0xF8
    [2024-06-27 09:52:59.262] [JET/DEBUG]i2c.c:readAllReg()(575):[20][14] Buf[0]:0xB
    [2024-06-27 09:52:59.269] [JET/DEBUG]i2c.c:readAllReg()(575):[20][14] Buf[1]:0x0
    [2024-06-27 09:52:59.278] [JET/DEBUG]i2c.c:readAllReg()(575):[20][14] Buf[2]:0x0
    [2024-06-27 09:52:59.290] [JET/DEBUG]i2c.c:readAllReg()(575):[20][14] Buf[3]:0x0
    [2024-06-27 09:52:59.290] [JET/DEBUG]i2c.c:readAllReg()(575):[20][14] Buf[4]:0x0
    [2024-06-27 09:52:59.303] [JET/DEBUG]i2c.c:readAllReg()(575):[20][14] Buf[5]:0x0
    [2024-06-27 09:52:59.305] [JET/DEBUG]i2c.c:readAllReg()(575):[20][14] Buf[6]:0x0
    [2024-06-27 09:52:59.320] [JET/DEBUG]i2c.c:readAllReg()(575):[20][14] Buf[7]:0x0
    [2024-06-27 09:52:59.320] [JET/DEBUG]i2c.c:readAllReg()(575):[20][14] Buf[8]:0x0
    [2024-06-27 09:52:59.323] [JET/DEBUG]i2c.c:readAllReg()(575):[20][14] Buf[9]:0x0
    [2024-06-27 09:52:59.338] [JET/DEBUG]i2c.c:readAllReg()(575):[20][14] Buf[10]:0x0
    [2024-06-27 09:52:59.338] [JET/DEBUG]i2c.c:readAllReg()(575):[20][14] Buf[11]:0x0
    [2024-06-27 09:53:00.362] [JET/DEBUG]i2c.c:readAllReg()(575):[20][16] Buf[0]:0xB
    [2024-06-27 09:53:00.368] [JET/DEBUG]i2c.c:readAllReg()(575):[20][16] Buf[1]:0x8
    [2024-06-27 09:53:00.378] [JET/DEBUG]i2c.c:readAllReg()(575):[20][16] Buf[2]:0x0
    [2024-06-27 09:53:00.389] [JET/DEBUG]i2c.c:readAllReg()(575):[20][16] Buf[3]:0x0
    [2024-06-27 09:53:00.391] [JET/DEBUG]i2c.c:readAllReg()(575):[20][16] Buf[4]:0x0
    [2024-06-27 09:53:00.407] [JET/DEBUG]i2c.c:readAllReg()(575):[20][16] Buf[5]:0x0
    [2024-06-27 09:53:00.407] [JET/DEBUG]i2c.c:readAllReg()(575):[20][16] Buf[6]:0x8
    [2024-06-27 09:53:00.409] [JET/DEBUG]i2c.c:readAllReg()(575):[20][16] Buf[7]:0x0
    [2024-06-27 09:53:00.424] [JET/DEBUG]i2c.c:readAllReg()(575):[20][16] Buf[8]:0x0
    [2024-06-27 09:53:00.424] [JET/DEBUG]i2c.c:readAllReg()(575):[20][16] Buf[9]:0x0
    [2024-06-27 09:53:00.432] [JET/DEBUG]i2c.c:readAllReg()(575):[20][16] Buf[10]:0x0
    [2024-06-27 09:53:00.436] [JET/DEBUG]i2c.c:readAllReg()(575):[20][16] Buf[11]:0x0
    [2024-06-27 09:53:01.461] [JET/DEBUG]i2c.c:readAllReg()(575):[20][18] Buf[0]:0xB
    [2024-06-27 09:53:01.467] [JET/DEBUG]i2c.c:readAllReg()(575):[20][18] Buf[1]:0x0
    [2024-06-27 09:53:01.477] [JET/DEBUG]i2c.c:readAllReg()(575):[20][18] Buf[2]:0x0
    [2024-06-27 09:53:01.488] [JET/DEBUG]i2c.c:readAllReg()(575):[20][18] Buf[3]:0x0
    [2024-06-27 09:53:01.490] [JET/DEBUG]i2c.c:readAllReg()(575):[20][18] Buf[4]:0x0
    [2024-06-27 09:53:01.506] [JET/DEBUG]i2c.c:readAllReg()(575):[20][18] Buf[5]:0x0
    [2024-06-27 09:53:01.506] [JET/DEBUG]i2c.c:readAllReg()(575):[20][18] Buf[6]:0x0
    [2024-06-27 09:53:01.508] [JET/DEBUG]i2c.c:readAllReg()(575):[20][18] Buf[7]:0x0
    [2024-06-27 09:53:01.522] [JET/DEBUG]i2c.c:readAllReg()(575):[20][18] Buf[8]:0x0
    [2024-06-27 09:53:01.522] [JET/DEBUG]i2c.c:readAllReg()(575):[20][18] Buf[9]:0x0
    [2024-06-27 09:53:01.534] [JET/DEBUG]i2c.c:readAllReg()(575):[20][18] Buf[10]:0x0
    [2024-06-27 09:53:01.534] [JET/DEBUG]i2c.c:readAllReg()(575):[20][18] Buf[11]:0x0
    [2024-06-27 09:53:01.557] [JET/DEBUG]i2c.c:readAllReg()(575):[20][1A] Buf[0]:0x5
    [2024-06-27 09:53:01.558] [JET/DEBUG]i2c.c:readAllReg()(575):[20][1A] Buf[1]:0x7D
    [2024-06-27 09:53:01.569] [JET/DEBUG]i2c.c:readAllReg()(575):[20][1A] Buf[2]:0x0
    [2024-06-27 09:53:01.571] [JET/DEBUG]i2c.c:readAllReg()(575):[20][1A] Buf[3]:0x20
    [2024-06-27 09:53:01.586] [JET/DEBUG]i2c.c:readAllReg()(575):[20][1A] Buf[4]:0x0
    [2024-06-27 09:53:01.586] [JET/DEBUG]i2c.c:readAllReg()(575):[20][1A] Buf[5]:0x0
    [2024-06-27 09:53:01.607] [JET/DEBUG]i2c.c:readAllReg()(575):[20][26] Buf[0]:0x5
    [2024-06-27 09:53:01.608] [JET/DEBUG]i2c.c:readAllReg()(575):[20][26] Buf[1]:0x80
    [2024-06-27 09:53:01.620] [JET/DEBUG]i2c.c:readAllReg()(575):[20][26] Buf[2]:0x0
    [2024-06-27 09:53:01.622] [JET/DEBUG]i2c.c:readAllReg()(575):[20][26] Buf[3]:0x0
    [2024-06-27 09:53:01.636] [JET/DEBUG]i2c.c:readAllReg()(575):[20][26] Buf[4]:0x0
    [2024-06-27 09:53:01.636] [JET/DEBUG]i2c.c:readAllReg()(575):[20][26] Buf[5]:0x40
    [2024-06-27 09:53:03.670] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[0]:0x11
    [2024-06-27 09:53:03.674] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[1]:0x2
    [2024-06-27 09:53:03.685] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[2]:0x0
    [2024-06-27 09:53:03.693] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[3]:0x2F
    [2024-06-27 09:53:03.696] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[4]:0x0
    [2024-06-27 09:53:03.713] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[5]:0x0
    [2024-06-27 09:53:03.713] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[6]:0x0
    [2024-06-27 09:53:03.716] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[7]:0x0
    [2024-06-27 09:53:03.727] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[8]:0x0
    [2024-06-27 09:53:03.727] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[9]:0x0
    [2024-06-27 09:53:03.739] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[10]:0x0
    [2024-06-27 09:53:03.741] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[11]:0x0
    [2024-06-27 09:53:03.756] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[12]:0x0
    [2024-06-27 09:53:03.756] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[13]:0x0
    [2024-06-27 09:53:03.765] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[14]:0x0
    [2024-06-27 09:53:03.774] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[15]:0x0
    [2024-06-27 09:53:03.778] [JET/DEBUG]i2c.c:readAllReg()(575):[20][28] Buf[16]:0x0
    [2024-06-27 09:53:03.793] [JET/DEBUG]i2c.c:readAllReg()(575):[20][29] Buf[0]:0x4
    [2024-06-27 09:53:03.805] [JET/DEBUG]i2c.c:readAllReg()(575):[20][29] Buf[1]:0xD2
    [2024-06-27 09:53:03.818] [JET/DEBUG]i2c.c:readAllReg()(575):[20][29] Buf[2]:0x50
    [2024-06-27 09:53:03.821] [JET/DEBUG]i2c.c:readAllReg()(575):[20][29] Buf[3]:0x90
    [2024-06-27 09:53:03.821] [JET/DEBUG]i2c.c:readAllReg()(575):[20][29] Buf[4]:0x47
    [2024-06-27 09:53:03.843] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2D] Buf[0]:0x5
    [2024-06-27 09:53:03.845] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2D] Buf[1]:0x0
    [2024-06-27 09:53:03.855] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2D] Buf[2]:0x0
    [2024-06-27 09:53:03.858] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2D] Buf[3]:0xF0
    [2024-06-27 09:53:03.874] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2D] Buf[4]:0xC2
    [2024-06-27 09:53:03.874] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2D] Buf[5]:0xC1
    [2024-06-27 09:53:09.933] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[0]:0x31
    [2024-06-27 09:53:09.939] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[1]:0x66
    [2024-06-27 09:53:09.949] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[2]:0x33
    [2024-06-27 09:53:09.958] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[3]:0x62
    [2024-06-27 09:53:09.961] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[4]:0x38
    [2024-06-27 09:53:09.976] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[5]:0x61
    [2024-06-27 09:53:09.976] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[6]:0x36
    [2024-06-27 09:53:09.988] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[7]:0x38
    [2024-06-27 09:53:09.990] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[8]:0x39
    [2024-06-27 09:53:10.014] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[9]:0x35
    [2024-06-27 09:53:10.014] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[10]:0x39
    [2024-06-27 09:53:10.014] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[11]:0x61
    [2024-06-27 09:53:10.018] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[12]:0x35
    [2024-06-27 09:53:10.030] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[13]:0x35
    [2024-06-27 09:53:10.033] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[14]:0x35
    [2024-06-27 09:53:10.046] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[15]:0x33
    [2024-06-27 09:53:10.049] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[16]:0x35
    [2024-06-27 09:53:10.049] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[17]:0x34
    [2024-06-27 09:53:10.065] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[18]:0x30
    [2024-06-27 09:53:10.065] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[19]:0x64
    [2024-06-27 09:53:10.079] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[20]:0x62
    [2024-06-27 09:53:10.083] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[21]:0x39
    [2024-06-27 09:53:10.083] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[22]:0x36
    [2024-06-27 09:53:10.093] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[23]:0x63
    [2024-06-27 09:53:10.095] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[24]:0x36
    [2024-06-27 09:53:10.109] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[25]:0x34
    [2024-06-27 09:53:10.109] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[26]:0x37
    [2024-06-27 09:53:10.120] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[27]:0x61
    [2024-06-27 09:53:10.135] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[28]:0x31
    [2024-06-27 09:53:10.139] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[29]:0x35
    [2024-06-27 09:53:10.139] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[30]:0x34
    [2024-06-27 09:53:10.149] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[31]:0x65
    [2024-06-27 09:53:10.149] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[32]:0x65
    [2024-06-27 09:53:10.160] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[33]:0x63
    [2024-06-27 09:53:10.163] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[34]:0x37
    [2024-06-27 09:53:10.179] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[35]:0x62
    [2024-06-27 09:53:10.179] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[36]:0x62
    [2024-06-27 09:53:10.183] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[37]:0x31
    [2024-06-27 09:53:10.198] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[38]:0x5F
    [2024-06-27 09:53:10.198] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[39]:0x30
    [2024-06-27 09:53:10.206] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[40]:0x30
    [2024-06-27 09:53:10.218] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[41]:0x36
    [2024-06-27 09:53:10.218] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[42]:0x32
    [2024-06-27 09:53:10.232] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[43]:0x30
    [2024-06-27 09:53:10.232] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[44]:0x32
    [2024-06-27 09:53:10.240] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[45]:0x32
    [2024-06-27 09:53:10.249] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[46]:0x0
    [2024-06-27 09:53:10.251] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[47]:0x0
    [2024-06-27 09:53:10.265] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[48]:0x0
    [2024-06-27 09:53:10.265] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2E] Buf[49]:0x0
    [2024-06-27 09:53:15.318] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[0]:0x28
    [2024-06-27 09:53:15.325] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[1]:0x54
    [2024-06-27 09:53:15.337] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[2]:0x50
    [2024-06-27 09:53:15.339] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[3]:0x53
    [2024-06-27 09:53:15.354] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[4]:0x36
    [2024-06-27 09:53:15.354] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[5]:0x35
    [2024-06-27 09:53:15.363] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[6]:0x39
    [2024-06-27 09:53:15.367] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[7]:0x39
    [2024-06-27 09:53:15.383] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[8]:0x32
    [2024-06-27 09:53:15.383] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[9]:0x20
    [2024-06-27 09:53:15.385] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[10]:0x48
    [2024-06-27 09:53:15.404] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[11]:0x57
    [2024-06-27 09:53:15.404] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[12]:0x30
    [2024-06-27 09:53:15.406] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[13]:0x30
    [2024-06-27 09:53:15.421] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[14]:0x43
    [2024-06-27 09:53:15.421] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[15]:0x31
    [2024-06-27 09:53:15.431] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[16]:0x46
    [2024-06-27 09:53:15.435] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[17]:0x57
    [2024-06-27 09:53:15.449] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[18]:0x46
    [2024-06-27 09:53:15.449] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[19]:0x38
    [2024-06-27 09:53:15.458] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[20]:0x30
    [2024-06-27 09:53:15.461] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[21]:0x39
    [2024-06-27 09:53:15.477] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[22]:0x2E
    [2024-06-27 09:53:15.477] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[23]:0x31
    [2024-06-27 09:53:15.487] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[24]:0x2E
    [2024-06-27 09:53:15.489] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[25]:0x30
    [2024-06-27 09:53:15.505] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[26]:0x30
    [2024-06-27 09:53:15.505] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[27]:0x5F
    [2024-06-27 09:53:15.507] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[28]:0x30
    [2024-06-27 09:53:15.522] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[29]:0x30
    [2024-06-27 09:53:15.522] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[30]:0x30
    [2024-06-27 09:53:15.533] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[31]:0x34
    [2024-06-27 09:53:15.534] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[32]:0x5A
    [2024-06-27 09:53:15.551] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[33]:0x41
    [2024-06-27 09:53:15.551] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[34]:0x63
    [2024-06-27 09:53:15.560] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[35]:0x65
    [2024-06-27 09:53:15.571] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[36]:0x53
    [2024-06-27 09:53:15.574] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[37]:0x0
    [2024-06-27 09:53:15.587] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[38]:0x0
    [2024-06-27 09:53:15.591] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[39]:0x0
    [2024-06-27 09:53:15.591] [JET/DEBUG]i2c.c:readAllReg()(575):[20][2F] Buf[40]:0x0
    [2024-06-27 09:53:18.629] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[0]:0x35
    [2024-06-27 09:53:18.635] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[1]:0x5
    [2024-06-27 09:53:18.644] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[2]:0x0
    [2024-06-27 09:53:18.658] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[3]:0x0
    [2024-06-27 09:53:18.658] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[4]:0x0
    [2024-06-27 09:53:18.667] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[5]:0x0
    [2024-06-27 09:53:18.671] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[6]:0x0
    [2024-06-27 09:53:18.684] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[7]:0x0
    [2024-06-27 09:53:18.684] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[8]:0x0
    [2024-06-27 09:53:18.694] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[9]:0x0
    [2024-06-27 09:53:18.697] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[10]:0x0
    [2024-06-27 09:53:18.712] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[11]:0x0
    [2024-06-27 09:53:18.712] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[12]:0x0
    [2024-06-27 09:53:18.722] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[13]:0x0
    [2024-06-27 09:53:18.724] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[14]:0x0
    [2024-06-27 09:53:18.739] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[15]:0x0
    [2024-06-27 09:53:18.739] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[16]:0x0
    [2024-06-27 09:53:18.747] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[17]:0x0
    [2024-06-27 09:53:18.757] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[18]:0x0
    [2024-06-27 09:53:18.759] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[19]:0x0
    [2024-06-27 09:53:18.772] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[20]:0x0
    [2024-06-27 09:53:18.775] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[21]:0x0
    [2024-06-27 09:53:18.775] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[22]:0x0
    [2024-06-27 09:53:18.789] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[23]:0x0
    [2024-06-27 09:53:18.789] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[24]:0x0
    [2024-06-27 09:53:18.799] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[25]:0x0
    [2024-06-27 09:53:18.809] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[26]:0x0
    [2024-06-27 09:53:18.809] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[27]:0x0
    [2024-06-27 09:53:18.821] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[28]:0x0
    [2024-06-27 09:53:18.823] [JET/DEBUG]i2c.c:readAllReg()(575):[20][30] Buf[29]:0x0
    [2024-06-27 09:53:21.862] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[0]:0x35
    [2024-06-27 09:53:21.869] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[1]:0x0
    [2024-06-27 09:53:21.877] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[2]:0x0
    [2024-06-27 09:53:21.886] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[3]:0x0
    [2024-06-27 09:53:21.890] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[4]:0x0
    [2024-06-27 09:53:21.903] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[5]:0x0
    [2024-06-27 09:53:21.903] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[6]:0x0
    [2024-06-27 09:53:21.914] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[7]:0x0
    [2024-06-27 09:53:21.916] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[8]:0x0
    [2024-06-27 09:53:21.933] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[9]:0x0
    [2024-06-27 09:53:21.933] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[10]:0x0
    [2024-06-27 09:53:21.942] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[11]:0x0
    [2024-06-27 09:53:21.944] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[12]:0x0
    [2024-06-27 09:53:21.963] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[13]:0x0
    [2024-06-27 09:53:21.963] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[14]:0x0
    [2024-06-27 09:53:21.965] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[15]:0x0
    [2024-06-27 09:53:21.980] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[16]:0x0
    [2024-06-27 09:53:21.980] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[17]:0x0
    [2024-06-27 09:53:21.983] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[18]:0x0
    [2024-06-27 09:53:22.000] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[19]:0x0
    [2024-06-27 09:53:22.000] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[20]:0x0
    [2024-06-27 09:53:22.002] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[21]:0x0
    [2024-06-27 09:53:22.018] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[22]:0x0
    [2024-06-27 09:53:22.018] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[23]:0x0
    [2024-06-27 09:53:22.032] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[24]:0x0
    [2024-06-27 09:53:22.032] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[25]:0x0
    [2024-06-27 09:53:22.043] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[26]:0x0
    [2024-06-27 09:53:22.045] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[27]:0x0
    [2024-06-27 09:53:22.060] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[28]:0x0
    [2024-06-27 09:53:22.060] [JET/DEBUG]i2c.c:readAllReg()(575):[20][31] Buf[29]:0x0
    [2024-06-27 09:53:25.097] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[0]:0x3F
    [2024-06-27 09:53:25.104] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[1]:0x1
    [2024-06-27 09:53:25.115] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[2]:0xA8
    [2024-06-27 09:53:25.118] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[3]:0x2A
    [2024-06-27 09:53:25.133] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[4]:0x2C
    [2024-06-27 09:53:25.133] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[5]:0x91
    [2024-06-27 09:53:25.143] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[6]:0x1
    [2024-06-27 09:53:25.146] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[7]:0x20
    [2024-06-27 09:53:25.162] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[8]:0x2C
    [2024-06-27 09:53:25.162] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[9]:0xD1
    [2024-06-27 09:53:25.164] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[10]:0x2
    [2024-06-27 09:53:25.181] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[11]:0x0
    [2024-06-27 09:53:25.181] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[12]:0x2C
    [2024-06-27 09:53:25.190] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[13]:0xB1
    [2024-06-27 09:53:25.193] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[14]:0x4
    [2024-06-27 09:53:25.209] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[15]:0x0
    [2024-06-27 09:53:25.209] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[16]:0x41
    [2024-06-27 09:53:25.212] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[17]:0x6
    [2024-06-27 09:53:25.231] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[18]:0x0
    [2024-06-27 09:53:25.231] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[19]:0xF4
    [2024-06-27 09:53:25.233] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[20]:0x41
    [2024-06-27 09:53:25.248] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[21]:0x6
    [2024-06-27 09:53:25.248] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[22]:0x0
    [2024-06-27 09:53:25.259] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[23]:0x0
    [2024-06-27 09:53:25.263] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[24]:0x0
    [2024-06-27 09:53:25.277] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[25]:0x0
    [2024-06-27 09:53:25.280] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[26]:0x0
    [2024-06-27 09:53:25.280] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[27]:0x0
    [2024-06-27 09:53:25.297] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[28]:0x0
    [2024-06-27 09:53:25.297] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[29]:0x0
    [2024-06-27 09:53:25.300] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[30]:0x0
    [2024-06-27 09:53:25.316] [JET/DEBUG]i2c.c:readAllReg()(575):[20][32] Buf[31]:0x0
    [2024-06-27 09:53:28.345] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[0]:0x35
    [2024-06-27 09:53:28.352] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[1]:0x1
    [2024-06-27 09:53:28.363] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[2]:0x2C
    [2024-06-27 09:53:28.371] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[3]:0x91
    [2024-06-27 09:53:28.373] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[4]:0x1
    [2024-06-27 09:53:28.390] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[5]:0x10
    [2024-06-27 09:53:28.390] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[6]:0x2C
    [2024-06-27 09:53:28.399] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[7]:0xD1
    [2024-06-27 09:53:28.402] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[8]:0x2
    [2024-06-27 09:53:28.418] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[9]:0x0
    [2024-06-27 09:53:28.418] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[10]:0x2C
    [2024-06-27 09:53:28.421] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[11]:0xB1
    [2024-06-27 09:53:28.436] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[12]:0x4
    [2024-06-27 09:53:28.436] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[13]:0x0
    [2024-06-27 09:53:28.440] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[14]:0xF4
    [2024-06-27 09:53:28.461] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[15]:0x41
    [2024-06-27 09:53:28.461] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[16]:0x0
    [2024-06-27 09:53:28.463] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[17]:0x45
    [2024-06-27 09:53:28.478] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[18]:0x41
    [2024-06-27 09:53:28.478] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[19]:0x6
    [2024-06-27 09:53:28.481] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[20]:0x0
    [2024-06-27 09:53:28.495] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[21]:0x0
    [2024-06-27 09:53:28.495] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[22]:0x0
    [2024-06-27 09:53:28.504] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[23]:0x0
    [2024-06-27 09:53:28.507] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[24]:0x0
    [2024-06-27 09:53:28.523] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[25]:0x0
    [2024-06-27 09:53:28.523] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[26]:0x0
    [2024-06-27 09:53:28.534] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[27]:0x0
    [2024-06-27 09:53:28.537] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[28]:0x0
    [2024-06-27 09:53:28.550] [JET/DEBUG]i2c.c:readAllReg()(575):[20][33] Buf[29]:0x0
    [2024-06-27 09:53:28.566] [JET/DEBUG]i2c.c:readAllReg()(575):[20][34] Buf[0]:0x6
    [2024-06-27 09:53:28.569] [JET/DEBUG]i2c.c:readAllReg()(575):[20][34] Buf[1]:0x2C
    [2024-06-27 09:53:28.572] [JET/DEBUG]i2c.c:readAllReg()(575):[20][34] Buf[2]:0x91
    [2024-06-27 09:53:28.588] [JET/DEBUG]i2c.c:readAllReg()(575):[20][34] Buf[3]:0x1
    [2024-06-27 09:53:28.588] [JET/DEBUG]i2c.c:readAllReg()(575):[20][34] Buf[4]:0x23
    [2024-06-27 09:53:28.604] [JET/DEBUG]i2c.c:readAllReg()(575):[20][34] Buf[5]:0x0
    [2024-06-27 09:53:28.606] [JET/DEBUG]i2c.c:readAllReg()(575):[20][34] Buf[6]:0x2
    [2024-06-27 09:53:28.617] [JET/DEBUG]i2c.c:readAllReg()(575):[20][35] Buf[0]:0xC
    [2024-06-27 09:53:28.621] [JET/DEBUG]i2c.c:readAllReg()(575):[20][35] Buf[1]:0x2C
    [2024-06-27 09:53:28.634] [JET/DEBUG]i2c.c:readAllReg()(575):[20][35] Buf[2]:0xB1
    [2024-06-27 09:53:28.636] [JET/DEBUG]i2c.c:readAllReg()(575):[20][35] Buf[3]:0x4
    [2024-06-27 09:53:28.652] [JET/DEBUG]i2c.c:readAllReg()(575):[20][35] Buf[4]:0x13
    [2024-06-27 09:53:28.658] [JET/DEBUG]i2c.c:readAllReg()(575):[20][3F] Buf[0]:0x2
    [2024-06-27 09:53:28.670] [JET/DEBUG]i2c.c:readAllReg()(575):[20][3F] Buf[1]:0xD
    [2024-06-27 09:53:28.678] [JET/DEBUG]i2c.c:readAllReg()(575):[20][3F] Buf[2]:0x2
    [2024-06-27 09:53:28.689] [JET/DEBUG]i2c.c:readAllReg()(575):[20][40] Buf[0]:0x4
    [2024-06-27 09:53:28.700] [JET/DEBUG]i2c.c:readAllReg()(575):[20][40] Buf[1]:0x70
    [2024-06-27 09:53:28.710] [JET/DEBUG]i2c.c:readAllReg()(575):[20][40] Buf[2]:0x0
    [2024-06-27 09:53:28.714] [JET/DEBUG]i2c.c:readAllReg()(575):[20][40] Buf[3]:0x80
    [2024-06-27 09:53:28.730] [JET/DEBUG]i2c.c:readAllReg()(575):[20][40] Buf[4]:0x0
    [2024-06-27 09:53:28.734] [JET/DEBUG]i2c.c:readAllReg()(575):[20][69] Buf[0]:0x4
    [2024-06-27 09:53:28.742] [JET/DEBUG]i2c.c:readAllReg()(575):[20][69] Buf[1]:0x2
    [2024-06-27 09:53:28.753] [JET/DEBUG]i2c.c:readAllReg()(575):[20][69] Buf[2]:0x0
    [2024-06-27 09:53:28.755] [JET/DEBUG]i2c.c:readAllReg()(575):[20][69] Buf[3]:0x2
    [2024-06-27 09:53:28.775] [JET/DEBUG]i2c.c:readAllReg()(575):[20][69] Buf[4]:0x60
    [2024-06-27 09:53:29.787] [JET/DEBUG]i2c.c:readAllReg()(575):[20][72] Buf[0]:0xC
    [2024-06-27 09:53:29.793] [JET/DEBUG]i2c.c:readAllReg()(575):[20][72] Buf[1]:0x12
    [2024-06-27 09:53:29.803] [JET/DEBUG]i2c.c:readAllReg()(575):[20][72] Buf[2]:0x0
    [2024-06-27 09:53:29.816] [JET/DEBUG]i2c.c:readAllReg()(575):[20][72] Buf[3]:0x0
    [2024-06-27 09:53:29.819] [JET/DEBUG]i2c.c:readAllReg()(575):[20][72] Buf[4]:0x0
    [2024-06-27 09:53:29.832] [JET/DEBUG]i2c.c:readAllReg()(575):[20][72] Buf[5]:0xD
    [2024-06-27 09:53:29.836] [JET/DEBUG]i2c.c:readAllReg()(575):[20][72] Buf[6]:0xC
    [2024-06-27 09:53:29.836] [JET/DEBUG]i2c.c:readAllReg()(575):[20][72] Buf[7]:0x0
    [2024-06-27 09:53:29.853] [JET/DEBUG]i2c.c:readAllReg()(575):[20][72] Buf[8]:0x0
    [2024-06-27 09:53:29.855] [JET/DEBUG]i2c.c:readAllReg()(579):Reading all registers finished.

    Regards,

    Roy

  • Hi,

    Please provide PD log and the project file (.json) first so we can check if PD contract is established correctly.

    Regards

  • Hi Tommy,

    Sorry that I'm not expert here. How can I export the PD log and project file(.json)? I am using MCU to control TPS25751.

    Regards,

    Roy

  • Hi Tommy, Kevin,

    In addition, we don't use typeC PD, but only 5V/3A source/sink. And we also want to change to use 5V/1.5A source/sink in specific condition. And we plan to use I2C to control. May you help let me know how to do it?

    And let me know the information you need to check. Many thanks.


    Regards,

    Roy

  • Hi Tommy, Kevin,

    Do you have any update?

    Regards,

    Roy

  • Hi Kevin,

    Please see below .json file. 

    {
      "questionnaire": {
        "device": "TPS25751",
        "answers": [
          null,
          1,
          0,
          0,
          0,
          0,
          0,
          0,
          0,
          1,
          1,
          null,
          0,
          0,
          0,
          0,
          0,
          0,
          0
        ],
        "vendorId": "0000",
        "productId": "0000",
        "version": "1.0.0.2"
      }
    }

    Currently, we measure that the CC1 pin voltage is 1.68V when we connect to my cell phone. The charging current is around 1.8A. So I think that the maximum source current setting is 5V/3A. And my target is that change the max source current from 3A to 1.5A or lower(USB default current) I tried to change 0x29[1:0], but no effect. And the CC1 pin voltage is always 1.68V.

    I also tried to re-connect my cell phone, but useless. May you let me know how to fix it?

    Regards,

    Roy

  • Hi Kevin,

    Excuse me. It's pending for a while. May you help let me know your comments?

    Do I need to set more source PDO like 5V/1.5A to achieve my requirment?


    Roy

  • Hi Kevin,

    I think I find that why we can't limit the typeC current. In 0x29[1:0] the setting is ignored during an explicit USB PD contract, where the Rp value is used for collision avoidance as required by the USB PD spec.

    And I check the 0x3F[3:2] = '11'. So we can't limit the typeC current using the 0x29 register. It's aligned.

    But I'm not sure why it enter into mode of "explicit PD contract sets current". May you give me the comment?


    Regards,

    Roy

  • Hi Roy,

    Apologies for the delay here!

    But I'm not sure why it enter into mode of "explicit PD contract sets current". May you give me the comment?

    When you enter an "explicit PD contract", that means that there was actual PD negotiation via the CC lines in which a PD contract that would be in either the TX source or TX sink cap was selected. In that case, the current in the PDO is the one that is used.

    Thank you,

    Kevin