Other Parts Discussed in Thread: TLV61046
Tool/software:
We are designing a 5V to 24V boost converter using TLV61046 . We need 80mA output current . Is there any limitation on this . How this maximum current can be calculated
Hi Nikhilraj,
When the inductor is 10μH, the guaranteed max Iout is around 79mA, very close to your application.
When the inductor is 22μH, the guaranteed max Iout is around 98mA. So it can meet your application when 22μH inductor is used.
Regards
Lei