Other Parts Discussed in Thread: TPS25925, , TPS4811-Q1
Tool/software:
Hi Mark,
The path inductance at the input and at the output determine the need of TVS diode at the i/p and schottky diode at the output.
As you see in datasheet, Equation 18 gives the transient voltage spike generated at the input when the device breaks the fault current. This demands TVS with appropriate clamping voltage to keep the input voltage with in the abs. max. of the TPS25925 device. Similarly, schottky diode is needed to freewheel the o/p current to clamp the negative voltages at the output.
TVS diode SMBJ16A-13-F and schottky diode B320A-13-F are recommended. The attachment provides information about the selection of TVS diode
TVS Clamping in Hot-Swap Circuits.pdf
Best Regards,
Rakesh
What are the criteria for selecting the Schottky diode that would be placed on the output in parallel with the TVS diode ?
The answer above addresses the TVS selection but not the schottky selection. Is there a similar article explaining the selection of Schottky for the output rail in Hot-swap applications ?
Thanks