This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62442-Q1: current capability

Part Number: TPS62442-Q1


Tool/software:

Hello team,

Hope you are doing well.

My customer wants to replace Maxim 3-channel buck to our TPS62442-Q1, but not sure about the current capability.

The two channels' requirements are separately 3V3->1V(1.8A) and 3V3->1V35(2.2A)

It is showed we can supply 2A+2A or 1A+3A in our datasheet, I want to check if it can supply 1.8A+2.2A, is it total 4A current capability for our part? Can we divide according to application requirement? Or we need to control under limit strictly?

Thanks!