Tool/software:
Hello to All,
for a variant of a project of a power supply, we need to use 2 LM5149 in dual phase mode, as suggests the application circuit 4 at the paragraph 9.2.4 in figure 9.40 of data sheet (SNVSBV4A). But the FB pin will be connect not only to output voltage (of course) but also to a MCU using a few resistors in order to vary the output voltage. With one LM5149, it's easy to do.
But it's not clear how implement this on dual phase regulator.
In reference to the diagram before mentioned, the connection to MCU will be done on Primary LM5149, as in the same of single phase and this is ok.
But how connect the FB pin in the Secondary LM5149?
The same question on PFM/SYNC pin on Primary LM5149... In my diagram, base on single LM4159, this pin is connect to AVDD pin... Is it possible to use the same connection on Primary LM5149?
Thank You and Best Regards
Federico Battaglin