Part Number: TPS65400
Tool/software:
Hello,
My customer is testing the TPS65400 operation on a board they designed as shown in the circuit below.
When they measured VDDA, VDDG, and VDDD after inputting VIN 12V and CE high according to the device startup sequence below, the output values were as follows.
- VDDA & VDDG = 0V, VDDD = 1V

Q1. Please review whether there is a problem with the customer's circuit above.
Q2. VDDA, VDDG, and VDDD output voltages are abnormal. Please give us advice on where to check to ensure that the device operates properly.
Thank you.
JH