Other Parts Discussed in Thread: LM74930, , LM5149
Tool/software:
Hello to All,
we are finishing a project of power supply 27V up to 13A.
To protect the cuircuit against the polarity inversion of batteries (2x 12V ermetic PB, normally 7-18Ah, but can be up to 65Ah), we are evaluating LM74930 chip.
But I have to ask clarification of behaviour of this chip in these operations step:
1) power supply is connected to 230Vac, the batteries are connected and the battery charger is charging the batteries
2) disconnect the batteries to replace it, by user
3) connect the new batteries but with polarity inverted, by user
4) the power supply advise this problem with any any damage (of batteries and of powers upply) and without any blackout on outpiut (because the are powered by 230Vac)
5) the batteries are re-connect in right manner, by user. And all it's ok.
QUESTIONS:
A) can this chip do this?
B) how this mechanism works?
Thank You and Best Regards
Federico Battaglin