This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952EVM: BQ76952 RAM register

Part Number: BQ76952EVM
Other Parts Discussed in Thread: BQ76952, , BQSTUDIO

Tool/software:

Hello, 

I am working on BQ76952EVM, I have problem with BQ76952 RAM register. I don't want to do OTP programming because the config parameters are not completely ready. I can change some parameters.

Anyway, the technical reference manual says that the Bq76952 is host configurable. so I configured it via Bqstudio, but when I send the reset command or shutdown command, the RAM register settings of the BQ76952 back to default values.

Is there any method to avoid reverting this to default values?  Can config update be done permanently without do OTP?