Tool/software:
Hi,
I am thinking about using the high-side switch to control a solenoid.
I am in a power sensitive application, so I am looking for a Peak and hold solution.
On the solenoid datasheet data is like this:
Coil Resistance 289 ohm
Pull-In @ 20 dg C 7V, 18 mA @0 bar
Drop-Out @ 20 dg C 3V, 3.5 mA @6 bar
Power Rating 0.5W
The solenoid have diodes included(flyback)
The datasheet of TPS1H200A-Q1, show that the flyback diode should be place differently from directly on the solenoid.
So what do you suggest?
Extra info I need a solution for 8 valves and open to other suggestions.