Hello,
I've design a power supply board to supply a RF module with the TPS63030 but I've a problem. When power save is disable I've no problem but when it is enable I can't detect my RF module unless the output voltage is 3,3V. I think that TPS63030 doesn't suplly enough current in power save disable but I don't understand why.
The power consumption of this module is 3,3V and 20mA every second during 100µs and 10µA during in the rest of the time. The transmission of the data is 80mA during 200ms.
So the power consumption seems to be less than the maximum current that the TPS63030 can supply in power save mode
My power supply board can accept 2 power supply, one with an external 5V supply and the other with a 3,6V LiSoCl2 battery.
Find below my scheme. R3 and R4 is the couple of resistor I change when to change power save disable and enable.
Is it possible to help me to understand why it doesn't work in power save enable ?