Other Parts Discussed in Thread: LMG2100R026
Tool/software:
Hi, I have certain question related to LMG2100R044.
Requirement to disable the gate driver:
Can we use VCC (5V) cutoff to enable and disable the gate driver. Our requirement is to switch off gate driver IC when there is any safety related fault. One of the faults is short circuit of GaN FET, in this case we need to shut down gate driver within 2us after asserting fault signal to gate driver IC. Is VCC cutoff is good way to make sure output GaN FET is turned off quickly within 2us? Or we need to have different strategy for this e.g. have switch on input PWMs to gate driver that will be opened (PWM state 0) in short circuit fault assertion.
Thermal Characteristics of LMG2100:
We are using this part in BLDC motor driver application. We will have LMG2100 for each three phases of the motor. Our switching frequency is 50kHz and supply voltage will be maximum 36V. Driver shall supply 15Arms continuous to motor and peak of 30 - 35Arms for 4-5 sec max. Can LMG2100 will meet this requirement. We would be using heat sink, and that heat sink will be mounted to metal enclosure. Our ambient temperature would be max 50 – 60 degrees C. What is your recommendation for better thermal strategy? Is this right part or do you have any other suggestions.