Other Parts Discussed in Thread: TPS62933
Tool/software:
Dear TI Support Team,
I'm working on a project that requires a dual-output buck converter to power a 12V DC motor and a 5V MCU. The power source is a 16V-20V battery. My priorities are cost-effectiveness and readily available components.
Requirements:
- Input voltage: 16V to 20V (battery)
- Output 1: 12V, 2A to 3A (motor)
- Output 2: 5V, 1A to 2A (MCU)
- Low cost and readily available components preferred
Research and Questions:
I've researched TI's buck converter offerings and came across the TPS65270PWPR. However, the datasheet doesn't provide clear instructions on configuring the outputs for 12V and 5V.
My questions:
- Can the TPS65270PWPR be configured to meet my specific voltage requirements (12V and 5V outputs)? If so, could you please provide guidance on the configuration process?
- If the TPS65270PWPR is not suitable, could you recommend alternative TI buck converter options that meet my needs for a low-cost, dual-output solution with readily available components?
Additional Information:
- I have experience with basic soldering and component selection.
- Project deadline is approaching, so a prompt response would be greatly appreciated.
Thank you for your time and assistance.
Sincerely,
Dhruvit Bhimani