This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A20:入力電圧低下時のドロップアウト電圧は?

Part Number: TPS7A20

Tool/software:

TPS7A2029PDQNRを利用する予定です。
本製品は2.9V出力ですが、入力電圧が3Vに下がった場合、ドロップアウト電圧はどのくらいになりますか?
出力電流は20mA未満です。
また、6.5節の表の仕様値は、Vin = Vout + 0.3Vを前提としていると理解していますが、この条件を満たさない場合、どのパラメータが影響を受けるのでしょうか?