This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951: DC - DC Power Converter Design

Part Number: UCC28951
Other Parts Discussed in Thread: UCC28950, UCC28180

Tool/software:

Hello,  

We are currently designing a novel DC-DC Power converter for battery charging applications & IC UCC28951 Looks interesting choice. 

Desgin Perameter: 
Vin min - 80VDC, Vin nom - 300VDC, Vin max - 400VDC
Vout nov - 24VDC - 26VDC, Iout - 45A nom, 50A max
Topology - Phase-shifted full bridge

Befour moving further with design we have couple of question as per below, 
1. Is there any Excel Design tool for this chip? 
2. Is it possible to control output voltage and output current with this driver IC? 
3. Do you have any application note on how to control output voltage and output current.

Please let me know if you require any more clarity

Regards
Umang