This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z746: BAT_SN/SP

Part Number: BQ27Z746

Tool/software:

Hi Team,

Could you pls help check if my below understanding is correct or not?

1. BAT_SP/SN only provides an accurate Cell voltage collection method.

2. If this sampling method is used, connect BAT_SP/SN to an external sampling circuit, such as ADC. At the same time, configure it in RLO mode or Buffer mode, and use appropriate thresholds to set BDP, BDN, BCP, and BCN.

3. If this function is not applicable, float BAT_SP/SN. Since the default XCHG_RLO = 0, no configuration is required.

Regards,
Hailiang